STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM generation for RGB LED Strip using WS2812 protocol

So i am using STM32F401RE board where i have written the code to for a strip of RGB led working on the WS2812 protocol which is nothing but using 24 bit PWM waveform for 1 led in GRB format. Every time i enable the PWM channel using CCR1 register for...

DJ1 by Associate III
  • 5194 Views
  • 2 replies
  • 0 kudos

Resolved! Upgrade ST-Link on Nucleo-H563ZI not possible

Hello,I want to do some programming on the Nucleo-H563ZI development board and the CebeIDE tells me that I need to upgrade the firmware on the ST-LinkV3. When I try to upgrade it, I get an error message:Since then I'm not able to do anything. The boa...

BViet1_0-1690373857701.png
BViet.1 by Associate III
  • 3371 Views
  • 5 replies
  • 2 kudos

STM32F303 Timer - Count Mismatch

HiIm using TIM6 on the STM32F303 MCU with clock 64 MHz and PSC 63999.If the ARR set to 65000 and in non- interrupt mode, the below code HAL_TIM_Base_Start(&htim6); HAL_Delay(500); HAL_TIM_Base_Stop(&htim6); results in CNT value of ~500 as expected.Ho...

PR.19 by Associate II
  • 1731 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F103C8T6 - no DAC?

I  had started an STM32F103C8T6 project in STM32CubeIDE. Now I wanted to use a DAC to output an analog signal from an internally stored wavetable.I don't see any DAC when opening the IOC editor. Doesn't the F103 have any DACs?

stm32h745 phy

hi, i want to implement ethernet communication between two stm32 boards without using phy, but only gpio's connected by jumpers. how can i disable the phy?

Ilay2002 by Associate
  • 1609 Views
  • 3 replies
  • 0 kudos

Impedance control for high speed SPI

Hello,We are a company making medical air transport containers. We use ST micro-controllers (STM32L562ZET6Q) to track, monitor and control our containers around the world.We are having issues with signal integrity between our micro-controller and our...

New batch 3MHz.jpg New batch 13MHz.jpg Old batch 13MHz.jpg
sagan by Associate
  • 4654 Views
  • 4 replies
  • 1 kudos

Resolved! STM32U599NJH6Q

Is this device in the witness protection program? Anglia cannot export the device outside the UK. Contacts for ST office in Canada are not listed. Good job. DK / Mouser list prices at 2-3x those on Anglia with 0 stock and ETA of the end of this year....

Mon2 by Senior III
  • 1545 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.