STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B0 ROM Bootloader USB DFU

Hi,I have been able to use the option bytes to configure the Nucleo-G0B1RE to jump straight into the ROM bootloader on powerup and I can see the DFU on Cube Programmer, however on our target board with a G0B0 using the same user option bytes settings...

SageTech by Associate
  • 2584 Views
  • 1 replies
  • 0 kudos

Resolved! In Clock Source BYPASS mode, can we use the OSC_OUT as GPIO?

Hello Community,We are using MEMS OScillator for the clock source for STM32G474 MCU. And are unsure if we can use the OSC_OUT pin as a GPIO pin when using the MCU in Clock Source BYPASS mode.The datasheet mentions we can, I, however, would like to co...

Chubs by Senior
  • 4256 Views
  • 6 replies
  • 3 kudos

How to configure AHB and APB for STOP Mode on STM32L4?

Hi,I was following @Laurids_PETERSEN post on his low power ThreadX example (Part 2 ThreadX Low power Project ). I noticed his sample code, Snippet 11 on Enter Low Power mode configured the APB ENR, AHB ENR in RUN mode and then disabled all the periph...

MD'Si.1 by Associate III
  • 2437 Views
  • 1 replies
  • 0 kudos

Multi ADC READ

I am trying to read Analog voltage from two different channel one is mains supply and another is battery voltage.But I am getting both values same in live expression window.Does my config wong.Pls helpvoid ADC_Mains(void) { ADC_ChannelConfTypeDef s...

meena by Associate III
  • 2241 Views
  • 1 replies
  • 0 kudos

stm32 pwm intrupt / hal handler

hello i m using tim1 to generate pwm and using center alligned mode 1 , timer go to 0 to 1800 then 1800 to zero for one pwm cycle and generate 2 intrrupts HAL_TIM_Base_Start_IT(&htim1); //intrrupt i am using//handler is void HAL_TIM_PeriodElapsedCall...

ahmash by Associate III
  • 1005 Views
  • 1 replies
  • 0 kudos

Resolved! GPIO, ADC and DAC not simultaneous

I am using stm32 g071 and what I have done in the code is to toggle pin and send the value through adc and finally output through dac. Theoretically, the GPIO output and DAC output should be simultaneous but due to processing time and all, there will...

Screenshot (48).png
RShre.2 by Associate III
  • 6044 Views
  • 13 replies
  • 1 kudos

Resolved! FDCAN problems on STM32G4

 I am developing a new project for the STM32G474 processor using the STM32G474E-EVAL1 board but am having a problem with FDCAN. I have two issues:1. I configure FDCAN and use the function HAL_FDCAN_AddMessageToTxFifoQ but the queue quickly fills up a...

RickN by Associate
  • 7467 Views
  • 3 replies
  • 1 kudos

Disturbance in MIPI DSI Output Image

Hi EveryOneBy Using DSI in Video Mode, It makes this disturbance in out image, What's the Main Source of this Problem:1. PCB Design (It's Two Layer Board, I tried My best to route it as short as possible)2. Noise in Ext RAM Data (Using EXT RAM as Fra...

MGH2023 by Associate
  • 1622 Views
  • 1 replies
  • 0 kudos

Resolved! Timer triggered DMA to GPIO for soft PWM

I'm trying to to generate a PWM signal on a GPIO without PWM capability on a STM32F47. To achieve this, I want to have a timer triggered DMA transfer to the GPIO BSRR register.Looking at the bus matrix, it seems that I need to use the DMA2 controller...

damanuel by Associate II
  • 3376 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.