STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Measuring capacitance using an 8-pin STM32

Hi,I designed a circuit using an 8-pin PIC microcontroller, which I would like to replace by a more advanced model.Being a total STM32 neophite, I wante to know if there is an 8-pin device offering the following features (* means the feature is alrea...

i4004 by Associate
  • 3255 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743: changes in 480MHz version?

Can someone please point me at a document that identifies any changes in the STM32H743 between the original 400MHz capable version and the latest 480MHz versionThanks

Resolved! ADC Readings Effected by Capacitors?

Hello,  I am new to ST boards, so please bear with me! I am trying to get a vibration reading from a beam using a piezoelectric sensor through an analog pin (ADC reading). I noticed in experiment that the timing of the piezoelectric sensor was not qu...

aab_2-1690703659000.png aab_0-1690703397957.png
aab by Associate
  • 3682 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H7 Synchronous USART receiving problem with DMA

Hello, in my project I need to read an encoder that clocks out data with clock burst. For this I decided to use UART with clock generation and DMA. (I also mixed up RX from one UART to another , but this is not a problem if request happens at the sam...

image.png image.png
Linas L by Senior II
  • 3157 Views
  • 5 replies
  • 2 kudos

Resolved! ADC and pullup/pulldown

Hi, for a STM32F303RE I configured a pin as an ADC input. I want to use the pullup/pulldown resistors as a voltage divider for an offset voltage. I tried to switch on both in ADC mode, that did not work. Everything is fine with the pin configured as ...

DetlefS by Senior
  • 16726 Views
  • 8 replies
  • 0 kudos

Resolved! Internal temperature sensor maximum sample rate specification for the stm32l4 series?

The ADC counts returned by the internal temperature sensor appear to depend on the sampling frequency.  In other words, it looks like the temperature sensor can be read too fast (with or without oversampling) to give incorrect temperature readings.  ...

UART DMA and SPI DMA problems on STM32G0B0

Hi all,I have an system that reads data form an external ADC via SPI DMA, i send the StartConversion CMD and when it's done i get and IRQ so i can read the register. I also have an UART communication that polls every 2sec for the new data, I have the...

PieterInHetBos_0-1690462554611.png PieterInHetBos_5-1690462665926.png PieterInHetBos_2-1690462602722.png PieterInHetBos_6-1690462685844.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.