2023-07-28 5:43 AM
hello i m using tim1 to generate pwm and using center alligned mode 1 , timer go to 0 to 1800 then 1800 to zero for one pwm cycle and generate 2 intrrupts
HAL_TIM_Base_Start_IT(&htim1); //intrrupt i am using
//handler is
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{//update happens here
}
while i need one intrrupt for one pwm cycle when timer goes 1800 to zero
what intrrupt and which handler do i need ?please help
2023-07-28 6:34 AM
In center-aligned (i.e. up-down) mode, you can't avoid Update being generated at both at top and bottom of the count.
But can use one of the center-aligned modes which generate output compare event only on one of the directions (i.e. TIMx_CR1.CMS=0b01 or 0b10), and use an appropriately set CC channel and its interrupt.
I don't know how to set this in Cube, I don't use Cube/CubeMX.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.