2023-08-05 7:16 PM
Hi,
We are working on a project based on the x-cube-aws package. I used the script from the GitHub STM32U5 AWS Virtual workshop to setup the project. The script STM32U5_AWS_VWS_PrereqCheck.ps1 runs successfully.
I got the error below when building the original project --- b_u585i_iot02a_tfm.
Calling cmake for artifact: tfm_build/.ready due to prereq: C:/temp/STM32CubeExpansion_Cloud_AWS_V3.0.0/Middleware/ARM/mbedtls/0003-Disable-export-MbedTLSTargets.patched C:/temp/STM32CubeExpansion_Cloud_AWS_V3.0.0/Middleware/ARM/mbedtls/0002-Enable-crypto-code-sharing-between-independent-binar.patched C:/temp/STM32CubeExpansion_Cloud_AWS_V3.0.0/Middleware/ARM/mbedtls/0001-BUILD-Update-IAR-support-in-CMakeLists.txt.patched
OSTYPE: ms/windows
OSTYPE: ms/windows
CMake Error at CMakeLists.txt:62 (message):
SETTING CMAKE_TOOLCHAIN_FILE no longer accepts relative paths. Please
supply an absolute path or instead use TFM_TOOLCHAIN_FILE (which does
accept relative paths)
-- Configuring incomplete, errors occurred!
I did change the path in the file tfm.mk to absolute path and the error is still there. How to resolve this ?
-DTFM_TOOLCHAIN_FILE=C:/temp/STM32CubeExpansion_Cloud_AWS_V3.0.0/Middleware/ARM/trusted-firmware-m/toolchain_GNUARM.cmake \
sliu1314
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.