STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reading from LCD Display. (Without I2C)

I don't understand how to use these two display modes:Read Busy Flag and Address CounterRead Data from RAMDatasheet LCD2004AI can describe how writing to DDRAM works. First, I put the cursor on the display where I want to write the character: LCD_Sen...

tim.png png.png
MMust.5 by Senior II
  • 9517 Views
  • 13 replies
  • 11 kudos

STM32H757 ST-link locked by ITSELF

I am working on STM32H757i-eval board. It worked well until this morning when it displayed "Error in initializing ST-Link device, Reason (4) No device found on target" at the time I was burning an image to it through the ST-link on stm32CubeIDE. Then...

Leoq by Associate II
  • 1709 Views
  • 1 replies
  • 0 kudos

FDCAN in Nucleo-U575Zi-q

Hello,  I am trying to Use FDCAN For Nucleo-u575Zi-Q , I already Configured two Stm32 emulation board with the same code one send data and other is receiving data , I did all init Functions and Enable interrupt when receiving data but non of this buf...

Resolved! STM32H563 ADC

When configuring ADC1 with STm32CubeIDE I see no IN2 or IN6. Why? 

mccabehm_0-1691510635454.png

Error with ST Developper Cloud AI

Hello,The ST developper cloud website returns an error message when downloading the CubeIde project, and only on large neural networks. The error seems to be due to the api (https://stm32ai-cs.st.com/api/8.0.1/project/) returning a Gateway timeout 50...

_legacyfs_online_stmicro_images_0693W00000dDVBgQAO.png
R.SOLER by Associate
  • 2780 Views
  • 3 replies
  • 0 kudos

USB initialization for NUCLEO-H723ZG board

Hi,I have a problem when I try to use the USB-HS, in FS mode without ULPI, on the NUCLEO-H723ZG board. In HAL_PCD_MspInit() function for H7,  the pins are not initialized. And the USB doesn't work.But in the .IOC file, the USB_OTG_HS_DP and USB_OTG_H...

MonkEastman_0-1691469871934.png MonkEastman_1-1691469988386.png MonkEastman_2-1691470140430.png

Resolved! LOW POWER MODE

please help me to solve this .My prototype is going to stand by but never waking up.I have used WKUP4 how i can assign interrupts for this .void Enter_sleep(void) { //enable PWR control clock __HAL_RCC_PWR_CLK_ENABLE(); // Set SLEEPDEEP bit of C...

meena by Associate III
  • 1334 Views
  • 1 replies
  • 0 kudos

STM32H747I-DISCO USART issue

When i want to init uart8static void MX_USART8_UART_Init1(void){huart8.Instance = UART8;huart8.Init.BaudRate = 115200;huart8.Init.WordLength = UART_WORDLENGTH_8B;huart8.Init.StopBits = UART_STOPBITS_1;huart8.Init.Parity = UART_PARITY_NONE;huart8.Init...

wjian.2 by Associate III
  • 1513 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.