STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32h723vgh6 ethernet problem

Hi,I have some problems with LwIp on custom board. Cpu type - stm32h723vgh6, ethernet chip - adin1200ccpz.Phisical layer works fine (link led is up). I've generated cube project with UDP and ICMP support according to recommendations in example projec...

zemlemer by Associate
  • 2534 Views
  • 4 replies
  • 0 kudos

porting to qspi flash based - hardfault on unalinged access

Dear AllI got the job to port a existing app which was developed for stm32h743 with 2mb flash to a stm32h750 with 128kb flash and a 8MB qspi memory.I basically succeeded in having a ext boot rom scenario where i would start from flash , enable qspi a...

RobertW by Associate
  • 2419 Views
  • 3 replies
  • 0 kudos

CAN-FD reset timer counter on RX pin data?

tldr; Can I have a timer counter reset (once / one-shot) when the RX pin of a CAN-FD peripheral is activated, so I can later determine the exact time elapsed?I have a chain of ~8 STM32 devices on a ~2m CAN-FD bus. Several MCU part numbers (mostly G4)...

StefanH by Associate III
  • 993 Views
  • 0 replies
  • 0 kudos

Trying to identify noise on the I2C bus

I'm working on STM32G491RET on the I2C bus. I've noticed intermittent noise on SDA and sparse timing inconsistency on the SCL as pictured. Could someone advise as to the nature/cause/imact of this. 

20230808_175110.jpg
aydamzn by Associate
  • 4296 Views
  • 7 replies
  • 4 kudos

Resolved! STM32H750 Quad SPI Flash Dual Image

Hello together,we have a board with an STM32H750I connected to a W25Q128 Quad SPI flash. We have our application code on the Quad SPI flash and run our application via XiP. This works fine. Now we work on our bootloader to update the application code...

ESawa.1 by Senior
  • 5087 Views
  • 8 replies
  • 2 kudos

Resolved! STM32F4VE Board for Schematic Design CAD File

Hi,  I am reaching out to kindly request to get the CAD file of the STM32F4VE board. This CAD file would greatly facilitate the process of designing a customized schematic diagram of our project. Please help me to find out the cad file of the board.

Resolved! USB MSD/USB Stick example for STM32G4 Series

Hello, I have a STM32G4 evaluation board. My goal is to read and write to a USB thumb drive (pen drive/MSD device) using an STM32G4 microcontroller (bare-metal). When I look at the possible USB examples in the CubeIDE, I can't find any examples for M...

1.png
ewilliams by Associate II
  • 4532 Views
  • 2 replies
  • 2 kudos

Resolved! ATM90E26 SPI Driver for STM32G491

Hi,I am  working with AGM90E26 Energy meter with STM32G491 with SPI.I checked for the drivers but I didn't find. If possible can anyone please share the energy meter SPI driver/resource link of that driver. It will be helpfulThanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.