STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Murata SCA3300_d01 sensor SPI_DMA communication

I am using NUCLEO-L4R5ZI MCU to communicate with Murata SCA3300 sensor. As an initial step I am trying to read WHOAMI to check weather SPI communication is established. According to data sheet of the sensor returned value should be 51h but I am getti...

shub by Associate
  • 922 Views
  • 0 replies
  • 0 kudos

ST-Link/V3 MINIE / V3 Mods UART flash

I have a question for you. The STM32 F303 processor can be programmed using the UART interface. I have ST-Link/V3 MINIE and V3-Mods and I'm trying to flash the processor using UART (I know it's possible via SWD but I absolutely need UART) After conne...

yaawl by Associate II
  • 9176 Views
  • 6 replies
  • 2 kudos

Device firmware update over ble from STM32 to NRF device

Is this possible to update firmware from an STM32 device to NRF device over ble. Need step-by-step approach to achieve this. The update procedure includes, Prepare the firmware update, Transfer the firmware, Verify and execute the updated firmware.

leo123 by Associate
  • 860 Views
  • 0 replies
  • 0 kudos

Crypt AES GCM is not correct

i use STM32F439ZIT6U and activate crypt function like below capture   and use library function   status = HAL_CRYP_Encrypt(&hcryp, (uint32_t *)inputStr, sizeStr, (uint32_t *)outputStr, HAL_MAX_DELAY); But outpustStr does not come out correctly like...

화면 캡처 2023-08-08 163254.png
daniel97 by Associate
  • 1225 Views
  • 0 replies
  • 0 kudos

Motorola 1D Barcode Scanner using USB Host HID

In one of my projects I'm using USB Host with STM32F407, It's working fine for both keyboard and mouse but while using Motorola Barcode scanner i face some issue related to USB host ID as it keeps on changing. It will connect with " HID_Device " Id, ...

Can't wake up with RTC on certain period

Hello!I am trying to wake up STM32L4 from STOP2 mode on each 3 seconds using RTC.This is the RTC initialization code:static void MX_RTC_Init(void){/* USER CODE BEGIN RTC_Init 0 *//* USER CODE END RTC_Init 0 */RTC_TimeTypeDef sTime = {0};RTC_DateTypeD...

LMehm by Associate III
  • 1667 Views
  • 2 replies
  • 0 kudos

Resolved! Having a problem with the USART on my STM32WL55JC2.

I am having a problem with the USART on my STM32WL55JC2. I have configured the USART correctly, and I am using the correct pins, but the USART is not working.I have tried the following to troubleshoot the problem:I have checked the configuration of t...

ABell.5 by Associate II
  • 2232 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.