STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! High current draw in STOP mode when RTC Alarm has been used

We have a very weird behavior in a battery powered IoT device. We should have a very low STOP mode current draw of 1.4 uA @ 3 VCC. The problem is, as soon as we use the RTC Alarm just once and although the alarm already fired during NORMAL operation,...

Resolved! STM32F103RB program hangs after calling HAL_TIM_Base_Start_IT()

Hello, I am using the NUCLE-F103RB and the STM32CubeIDE for developing and testing code. After my latest code change the program does not return form the below call of HAL_TIM_Base_Start_IT(&htim3)."TEST1" is printed to the terminal, but "TEST2" is n...

Kmax18 by Senior II
  • 4085 Views
  • 5 replies
  • 4 kudos

Resolved! stm32f407 Programming parallelism error firing for no reason

I am using the stm32f4 discovery board and writing bare-metal drivers for the embedded flash memory.I am facing a strange problem when writing to flash memory, to save you time for reading code and when the error happens, here is the status:Before Er...

abdosalm_0-1691609290197.png abdosalm_1-1691609309480.png abdosalm_4-1691601763454.png abdosalm_5-1691601825030.png
abdosalm by Associate II
  • 3765 Views
  • 5 replies
  • 0 kudos

STM32F407 ADC Issue

Hello all,I'm using STM32F407 ADC1 with DMA enabled for sampling on 4 channels at same time, the configuration for these 4 channels are all same with DIV4 clock and 12Bit Resolution, but only 3 of them are working fine, and one channel always returns...

XLei.3 by Associate II
  • 3914 Views
  • 8 replies
  • 0 kudos

Resolved! STM32H7 max SDRAM clock speed for 480MHz

ST example uses 400MHz / 4 = 100MHz for SDRAM. What should the SDRAM clock be when the system is running at 480MHz? If we use 480/4 then it is 120Mhz for SDRAM, but datasheet shows max of 100MHz for SDRAM! Are we stuck running SDRAM at 60Mhz? Or run ...

Dat Tran by Senior II
  • 6951 Views
  • 6 replies
  • 2 kudos

STM32G0B1 system bootloader and GPIO conflicts

Hello,We have designed a board around a STM32G0B1CB where almost all the 48 pins are used for different stuff (lots of analog inputs, communication and PWM).It is not our first design with STM32 uC, but we are facing an issue here and I would like to...

Kraal by Lead
  • 5563 Views
  • 8 replies
  • 0 kudos

USING ADITIONAL USART IN STM32WL55

Hi ,I am trying to use 2 usart in stm32wl. But right now I am using Single uart which default PA2 and PA3 we can access through debug port, But I am trying to use through other gpios or pins through ttl But the output is not coming in terminal if I c...

L431 stops working after enabling DAC

I am trying to use the onboard DAC to generate a sine signal. The program runs without any problem on the Nucleo L432KC board but it would not work on our PCB with L431. As soon as the DAC is enabled with LL_DAC_Enable(DAC1, LL_DAC_CHANNEL_1); the pr...

ZJing by Associate III
  • 2342 Views
  • 2 replies
  • 0 kudos

inline assembly macro inconsistent

I am using the STM32F746VET6. I am aware that assembly instructions do not have a guaranteed in execution time, however I am surprised how consistently inconsistent my inline assembly macro is behaving. I'm really hoping there is just a mistake in th...

RBack.1 by Senior
  • 10571 Views
  • 14 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.