STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to detect what level digital input caused interupt

Hi  I have pin PA6 setup to interupt on high and low levels. I have done the following:GPIOA->MODER &= ~GPIO_MODER_MODE6; //PA6 as inputSYSCFG->EXTICR[1] &= ~SYSCFG_EXTICR2_EXTI6; //PA6EXTI->RTSR1 |= EXTI_RTSR1_RT6; //enable rising edgeEXTI->FTSR1 |=...

STM32F103ZET6 - Interface with LCD driver Ilitek ILI9341

Hi,I have inherited a project that utilizes Nuttx RTOS. This project is to change out the LCD display due to EoL. We are changing from Renesas R61580 Driver to Ilitek ILI9341. The existing driver is hooked up via 16-bit MCU command via the FSMC, with...

JT-88 by Associate
  • 1983 Views
  • 1 replies
  • 0 kudos

SDCard initialization issues

Hi everyone,I am encountering issues in sdcard initialization on my custom board.I am getting SDMMC_FLAG_CTIMEOUT error in SD_PowerON once the first CMD8: SEND_IF_COND is sent.Looking at signals and comparing with an identical custom board, you can s...

lukin_1-1692721035932.jpeg lukin_0-1692721024193.jpeg
lukin by Associate III
  • 977 Views
  • 0 replies
  • 0 kudos

Resolved! GND diference

There are no diference for conect to gnd in the left side o right side? 

wjian2_0-1692719089476.png
wjian.2 by Associate III
  • 1467 Views
  • 1 replies
  • 0 kudos

G.722 vocoder

Hello,I've seen the AN4229-how-to-implement-a-vocoder-solution note, which talks about support for G.711 and G.726. Does anyone know if anything is available specifically for G.722?Thanks

EC.3 by Associate III
  • 1138 Views
  • 0 replies
  • 0 kudos

How to index different GPIO ports in one array

hi everyone.I'm trying to index different GPIO ports and pins.  #define STEP1_HALF1_PORT GPIOA#define STEP2_HALF1_PORT GPIOB#define STEP3_HALF1_PORT GPIOA#define STEP4_HALF1_PORT GPIOC#define STEP5_HALF1_PORT GPIOBGPIO_TypeDef *Half1StepPortNum[5] = ...

Resolved! Micro Trace Buffer (MTB) on STM32U5 devices?

Dear STM CommunityIn order to ease our debugging, I would like to make use of the Micro Trace Buffer which seems to be integrated in the Cortex M33 Core (e.g. stated by STM here: https://www.st.com/content/st_com/en/arm-32-bit-microcontrollers/arm-co...

Stef2 by Associate III
  • 2086 Views
  • 1 replies
  • 0 kudos

Resolved! iwdg is not working while usb device is running.

Hi,My MCU us stm32f401rct6.This MCU has three UART and all UART are using for service. No console UART port :(So, I make a USB CDC device to use console port.But, iwdg is not working. When I use UART console port, while(1); occur watchdog reset. But,...

Paul.Lee by Associate III
  • 3471 Views
  • 6 replies
  • 0 kudos

SPI1 with DMA Overflow Issue

I have SPI1 setup as Receive Only Slave with DMA enabled.  I send 10 bytes from SPI2 ( to simulate a full duplex master uC )  and it works well the first time I transmit 10 bytes.  When I transmit 10 bytes a second time, SPI1's overflow flag gets set...

LMorr.3 by Senior II
  • 2498 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.