STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L433 STOP2 current draw higher than expected

We are working on a project which requires us to put our STM32L433 MCU's into a low power mode with memory retention(STOP2 mode). When measuring the IDD current draw on our NUCLEO-L433RC-P  in STOP2 mode, we found that at 1.8V VDD the current consump...

Andre_k_0-1692697191173.png e09eb428-f503-4536-991f-574e2002243d.jpg e5b9dd06-ab9b-4525-87ce-299759c8ee71.jpg
Andre_k by Associate III
  • 3296 Views
  • 5 replies
  • 2 kudos

eMMC stop and restart

hi all,we have an application that requires powering an eMMC down and then back up while the MCU keeps running. BackgroundWe're successfully using the eMMC connected to the SDMMC1 peripheral running on a 25MHz 8-bit bus, with ClockPowerSave ENABLED. ...

0690X00000AtWDRQA3.png 0690X00000AtWGkQAN.png
DShar.17 by Associate II
  • 2995 Views
  • 3 replies
  • 0 kudos

How can I get started with the TouchGFX platform?

I want to use the TouchGFX framework in my projects, but I have no idea where to start. I'd like to know where I can find the necessary information, from selecting the screen controller to programming. I hope you can help me with this. Thank you

WPazH by Associate II
  • 1871 Views
  • 1 replies
  • 0 kudos

STM32 L0 Flash Writing issues.

Hi ST Community,I have inherited a product that runs on a stm32L051k8 mcu, and I am having difficulty with using the onboard flash memory. On boot, the product checks a certain location in flash to see if there are some configuration settings stored ...

MCocke.1 by Associate
  • 2342 Views
  • 2 replies
  • 1 kudos

Resolved! [STM32F103] Send CAN message in CAN receive callback interrupt

Hello there,I am working with CAN on STM32F103. I want my MCU to send a message right when it receives a message so I put HAL_CAN_AddTxMessage function in HAL_CAN_RxFifo0MsgPendingCallback. I tried it with STM32F4 like this and it worked fine.void HA...

QTLe by Associate
  • 3075 Views
  • 3 replies
  • 1 kudos

Problem with SPI on bluepill module

SOLVED: was a problem with NSS pin, the code is GPIOA but NSS is GPIOB... thought I corrected it Hello, I am trying to read register on a RFM69HW transceiver, it uses SPI.I have used this module extensively. Works perfectly on arduinos, esp, and othe...

LLope.31 by Associate III
  • 2420 Views
  • 2 replies
  • 1 kudos

Attempting to change the UART port of a sample

Greetings,I want to compile the BLE Transparent Mode sample from the Cube (Version: 1.13.1Build: 17479_20230728_0839 (UTC)) for the STM32MMB module that has a different UART port from the default which is PB6/7.  Our design uses PA9/10 because we nee...

eleventen by Associate III
  • 1642 Views
  • 2 replies
  • 0 kudos

Resolved! SPI debugging stops after around 125 bytes being send

Hi STM forums,I use a stm32f205rct6tr for this projectin my project i need to send 1024 clock signals to the slave, the message inside is not inportant.but after sending around 125 bytes it stops debugging entirely, i checked it out with the oscillos...

Screenshot_159.png Screenshot_160.png Screenshot_161.png

Resolved! ATM32H747xi datasheet Table 9. Port A - Question

In the ATM32H747XI datasheet Table 9 on page 89...As I read this table... Examples are...Pin Name PA1 Alternate Function AF1 = TIM2_CH2Pin Name PA2 Alternate Function AF2 = TIM5_CH3Question 1:For PA0 AF1, there are two functions listed... TIM2_CH1/TI...

Will_iii by Associate II
  • 1882 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.