STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART in SPN5

Hello,I am using X-CUBE-SPN5 with F030R8 and IHM05A1 to control a stepper motor and it works well.I would now like to use UART with provided driver (stm32f0xx_hal_uart).Hence, I enabled UART use in stm32f0xx_hal_conf.h.To test UART integration, I am ...

user-stm by Associate II
  • 3718 Views
  • 6 replies
  • 0 kudos

Resolved! STM32U5 lower power mode in Threadx with trustzone enabled

Hi Team, I'm currently trying to enter low power mode mode stop 0,1,2,3 and standby mode with Trustzone enabled using Threadx. The device is entering low power mode when interrupt triggers the thread is not resuming it still in the low power mode. Is...

Gautham19 by Associate II
  • 2914 Views
  • 2 replies
  • 0 kudos

how to install linux

I am using IAR and stm32cubemx.how can i install linux os on stm32h743?I don't know howOtherwise, it would be much appreciated if you could provide a document or link

BPark.5 by Associate II
  • 4768 Views
  • 4 replies
  • 0 kudos

Resolved! JPEG Mode in DCMI

In your application note AN5020 and related to JPEG reception. i have some questions and hopefully you can answer them so every thing work. Each JPEG stream is divided into packets, which have programmable sizeWhat does JPEG Stream means? is it JPEG ...

MSale.1 by Senior
  • 3745 Views
  • 3 replies
  • 0 kudos

Resolved! FDCAN monitoring bus when MCU in sleep mode

Is it possible for STM32H5 to monitor the CAN bus when MCU is in sleep mode? Upon CAN bus activity detection, MCU automatically performing the wakeup sequence to be back in normal run mode.

Imre by Associate III
  • 4179 Views
  • 5 replies
  • 1 kudos

Resolved! I2C Master_Transmit error because of NAK

My setup is as follows: I have a NUCLEO-H563ZI with an STM32H563ZIT6 and I am communicating through I2C with the 6D IMU, ISM330DCL. Moreover the ISM330DCL is on the STEVAL-MKI182V2.My I2C-bus is very confusing. First I get everything set up exactly a...

ichbinGroot_0-1693862836060.png

Resolved! One bit shift in SPI communication on STM32H7

I'm working on SPI communication between two Nucleo-H743ZI boards. I'm using ST's HAL, and the SPI polling API HAL_SPI_TransmitReceive.It's working fine until a bandwith of 12Mbits/s (SPI kernel clock at 200Mhz and prescaler 16, the CPU is always at ...

Gpeti by Senior II
  • 7745 Views
  • 10 replies
  • 1 kudos

FUOTA IAP Updating Only Part of a Program

My goal is to implement an In-App Programmer (IAP) that can update part of our firmware from data we receive over a wireless network. We do not want to update the full firmware because it's too large and would take too long/consume too much power.I'm...

Cfaya.1 by Associate II
  • 1019 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.