2023-11-01 8:03 PM
Hi, I read input PWM signal from RC radiolink (done): duty_cycle range 675-1347
And now I want to convert this signal to analog to ON/OFF led, I used MAP funtions and I don't know how to move read_RC to ON led, something's like analogWrite (read_RC, Led);
uint32_t frequency, duty_cycle;
uint32_t capture_value;
uint32_t duty_cycle_min = 675;
uint32_t duty_cycle_max = 1347;
uint32_t read_RC;
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
if(htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
{
capture_value = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1);
if(capture_value)
{
frequency = SystemCoreClock/(capture_value);
duty_cycle = 10000 * HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_2)/capture_value;
}
}
}
while (1)
{
read_RC = MAP(duty_cycle, duty_cycle_min, duty_cycle_max, 0, 4294967295);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.