2023-11-01 10:46 AM
In our application, STM32 micro controller USART protocol is used as UART full duplex mode.
what will be the conditions to use USART as UART full duplex mode?
Already I have disabled CLKEN bit in USART_CR2 register.
Though, disabling CLKEN bit in USART_CR2 register still I am getting issue while transmitting data from micro controller.
the issue is the dock light is not receiving same data ,We verified but it is not the baudrate issue.
2023-11-01 12:28 PM
Show what you're sending, show what you're receiving, and the code / expected configuration.
Perhaps you can show the signalling on a scope or logic analyzer?
How is this wired up? CMOS and RS232 levels are different.
>>what will be the conditions to use USART as UART full duplex mode?
I supposed that you use independent functions that don't block?
2023-11-01 9:35 PM
Actually, I am configuring Bluetooth with STM32 micro controller
The protocol required to communicate with bluetooth is UART but I am using USART in my micro controller(Already I have disabled CLKEN bit in USART_CR2 register). I dont know what's the issue but while transmitting commands I am not receiving same commands at my bluetooth side .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.