2025-09-15 7:42 PM
I want to use N657B0 to drive VD55G0, and the camera side can already enter the Stream state. After I use the function HAL_DCMIPP_CSI_PIPE_Start, I track the variable csi_instance through single-step debugging and find that several bits in its SR1 register are inconsistent with the normal state. And I find the defination about these.The normal state is 1 but I get 0.Could you please tell me what the reason for this might be?
Is the issue caused by a voltage supply problem in the hardware connection, or by inadequate rate matching in the port?
2025-09-22 10:51 AM
@eureka May I ask what driver you use for the VD55G0 sensor, and where you got that from? I asked about this in this forum, and got an official answer from ST that a driver is not yet available.
Thanks, Michael
2025-11-20 6:05 AM
I wrote the driver code strictly according to the datasheet. Unfortunately, I haven't been able to get it working either.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.