STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G030k8 ADC sequencer set not fully configuarable

Hi I already asked for multi channel ADC in STM32G030K8 PA0,PA2,PA5,PA9,PA11,PA12.while debugging I am getting all ADC values as same if I made one by one its working properly Can any one help how to proceed with that.

meena by Associate III
  • 1742 Views
  • 2 replies
  • 0 kudos

STM32U5A9ZJY6QTR Pixel Resolution support

Hello all,What is the pixel resolution support of STM32U5A9ZJY6QTR MCU.I need support of 1080 x 1920 pixel resolution for max 6'' inch display with both MIPI DSI and RGB888 support.Any possible help. 

Ashu123 by Associate
  • 2051 Views
  • 2 replies
  • 0 kudos

STM32WB55 RDP protection level

Hello I am trying to flash code using openocd(through JTAG) in option byte RDP protection level is set to AA(0) but still openocd throwing error memory is write protected can not write on address 0x8000000. Hardware : STM32WB55 Nucleo boardOpenocd Ve...

DineshB by Associate III
  • 4606 Views
  • 7 replies
  • 0 kudos

Resolved! STM32G431KB Nucleo 32 - USART1 RX help

I'm trying to use USART1 for Async however I cannot send data to the board. I'm using an FTDI USB-UART converter cable to test, the Nucleo is sending correct data my PC data no problem.I can prove my code and terminal program on the PC works 2 way wi...

LiamRDS by Associate
  • 3320 Views
  • 4 replies
  • 1 kudos

How to change default UART Idle line Inactivity time

Hello There,I'm utilizing IDLE event functionality of UART and use HAL_UARTEx_ReceiveToIdle_IT() for it.The issue that I'm facing is that some times this API falsely detects an IDLE event upon reception (May be a Transmitter issue). So, to overcome t...

KAgga.1 by Associate III
  • 14008 Views
  • 13 replies
  • 0 kudos

Flash Read not working

I am using the SBSFU example in stm32l562edk devkit.I have modified flash_layout.h and I have added a 4 KB user data section in which I am trying to store user data from the application. I have ported a flash driver(read, write, erase) from the bootl...

PYada.1 by Associate III
  • 3923 Views
  • 4 replies
  • 0 kudos

Resolved! About CAN filter

HiMany CAN messages are flowing on the CAN bus.I would like to receive only ID 0x5C0 among these.Please let me know the suitable settings to receive only 0x5C0 as a hardware filter without any software intervention, without any load on the MCU.I wrot...

Ukazu by Associate III
  • 3418 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.