2023-11-19 11:27 PM
Hello all,
What is the pixel resolution support of STM32U5A9ZJY6QTR MCU.
I need support of 1080 x 1920 pixel resolution for max 6'' inch display with both MIPI DSI and RGB888 support.
Any possible help.
2023-11-20 2:23 AM
Hello @Ashu123 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you take a look at the AN4861 to calculate the supported resolution according to your project configurations.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-20 2:57 AM
It doesn't have the bandwidth to support FHD resolution.
Perhaps can get to 1024x768.
You need memory for the frame buffer, perhaps two, and DSI/MIPI 2-Lane at 1Gbps total.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.