STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! A question about F103C8T6 memory map.

I found in "Figure 11. Memory map" of "Datasheet - production data for STM32F103x8", the address span between Port A and Port B is 1024(0x4001 0c00 - 0x40010800 = 32*32 bits), while I found in "RM0041 - Reference manual STM32F100xx advanced Arm ® -ba...

MQi.1 by Senior II
  • 2616 Views
  • 1 replies
  • 2 kudos

STM32H563ZI : USB CDC issue

Hello , As per reference document added USB driver in firmware , but gives error at function USBD_SetClassConfig(pdev, cfgidx);added screenshot of error If ignore this error , USB Serial device port detected but failed to set transmission buffer stat...

stm32_error.png
pooja by Associate II
  • 3592 Views
  • 6 replies
  • 0 kudos

STM32F427 USB Vendor device

Hello all,For a first time i am trying to implement usb vendor device. I am using stm32 standard peripheral library. Basically  CDC class, having modified the interface recognition part. Can i have some direction what i am missing to implement. Here ...

Lachezar_0-1699868646627.png
Lachezar by Associate II
  • 2183 Views
  • 2 replies
  • 0 kudos

Resolved! U5 ENCODER in STOP2 does not update count

I'm using NUCLEO U575ZI with LPTIM1 configured as Quadrature ENCODER with 32kHz internal clockIn RUN mode peripheral works properly but when I switch in STOP2 mode peripheral doesn't count.I can assume the peripheral is powered ON because when I exit...

amoli.1 by Associate II
  • 2600 Views
  • 4 replies
  • 0 kudos

STM32L5: External loader does not work

Hi, With the STM32L562E-DK devoplement kit, I have developed a working touchGFX application without Trustzone. The external loader MX25LM51245G_STM32L562E-DK works as expected with STM32CubeProgrammer (version 2.14.0) However, I need trustzone, so I ...

Resolved! How to implement multiple interrupt timers using HAL libraries

I'm trying to get multiple timers with interrupts working on an STM32L462 using the provided HAL libraries in CubeIDE 1.14, but every time the chip comes out of reset, it crashes after starting the second timer. Here is the relevant code:  int main(v...

antfarmer by Associate III
  • 11420 Views
  • 8 replies
  • 2 kudos

writing to gpios on two different ports at the same time?

Hi.I'm testing gpios on many different ports at the same time.I'm testing buttom code.///////////////////////////////////////////////////////////////////////////////////////////////////////////////////__HAL_TIM_CLEAR_IT(&htim12, TIM_IT_CC1);GPIOE->BS...

JLee.21 by Associate II
  • 1292 Views
  • 1 replies
  • 1 kudos

Example for SMBus Host on STM32G031K8

hi,I'm looking for SMBus Host Controller on STM32G031K8.. The example is for different boards and when porting in done on my target I don't see any behavior as explained in the example.Kindly provide some pointers.

Resolved! No Interrupts with timer encoder function? Nucleo G431KBT6

I tried to make an interrupt work with encoder input on timer 1. It does not fire interrupts.Interrupts are activated (the code is reached).Are there simply no interrupts possible, or is it another problem that i have to figure out?

Tobe by Senior III
  • 1818 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.