2023-12-04 10:33 PM
This is the code i have generated using TIM2 CH1
could you please set the prescalar, period,pulse to get output every 5s
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 169;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 9999;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 9999;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
//motor1State = MC_GetSTMStateMotor1();
HAL_TIM_Base_Start(&htim2);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
//motor1Faults = MC_GetOccurredFaultsMotor1();
motor1Faults = MC_GetCurrentFaultsMotor1();
switch (motor1Faults)
{
case 0:
HAL_UART_Transmit_DMA(&huart2, "MC_NO_ERROR", 12);
break;
case 1:
HAL_UART_Transmit_DMA(&huart2, "MC_DURATION", 12);
break;
case 2:
HAL_UART_Transmit_DMA(&huart2, "MC_OVER_VOLT", 13);
break;
case 4:
HAL_UART_Transmit_DMA(&huart2, "MC_UNDER_VOLT", 14);
break;
case 8:
HAL_UART_Transmit_DMA(&huart2, "MC_OVER_TEMP", 13);
break;
case 10:
HAL_UART_Transmit_DMA(&huart2, "MC_START_UP", 12);
break;
case 20:
HAL_UART_Transmit_DMA(&huart2, "MC_SPEED_FDBK", 14);
break;
case 40:
HAL_UART_Transmit_DMA(&huart2, "MC_BREAK_IN", 12);
break;
case 80:
HAL_UART_Transmit_DMA(&huart2, "MC_SW_ERRORS",12);
break;
}
/* USER CODE END TIM2_Init 2 */
HAL_TIM_MspPostInit(&htim2);
}
2023-12-05 12:55 AM
Hello @soundarya_h_s,
Check the block diagram in your product datasheet, to know which bus the TIM2 is connected to (in your case it's APB1)
Here are the formulas you're going to need :
To calculate the TIM clock frequency: TIM Clock = APB TIM clock/ (PSC+1)
PSC = 170MHz/1MHz) - 1 = 169
To have an event every 5 seconds, you should set the ARR to (5s/1us) - 1 = 4,999,999
pulse value is not relevant since you're not using the timer in PWM mode
You also need to configure the timer to generate an interrupt on update event
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-05 1:18 AM
Hello @Sarra.S
can you provide the code for interrupt on update event
should i add callback function or what should i add in the interrupt
is the switch case should be present in the TIM2 init itself
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.