STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GreenPAK

Hi all,I'm starting to use GreenPAK devices... I use the SLG46826V version which is reprogrammable, and I want to take advantage of the possibility of programming it on board with the I2C of the STM micro. The device I read and write regarding the re...

MBosc.2 by Associate II
  • 1192 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F103C8T6 SPI

Hii all,First of all i am new to bluepill(stm32f103c8) and i want to use both the SPI1 & SPI2 for the same project .BUT i don't know how to use it i am using Arduino ide for code 

Kalp_13 by Associate
  • 1811 Views
  • 1 replies
  • 0 kudos

Resolved! Hardware timer interrupt for multiple delays(STM32g4)

Hi,I am using STM32G4 in my project. I need delays in my project multiple places. I am using hardware timer interrupt for delay. I am using TIM1 configured with 50 usec delay. HAL_TIM_Base_Start_IT(&htim1); HAL_TIM_PWM_Start_IT(&htim2, TIM_CHANNEL_2)...

Resolved! STM32L552CC program counter after bank swapping

Hello, I'm using a STM32L552CCT6. For firmware update I want to use the dual flash bank functionality of the controller.When switching the flash banks with the option bit SWAP_BANK in register FLASH_OPTR what happens to the program counter? Is he als...

dost by Associate II
  • 1950 Views
  • 3 replies
  • 0 kudos

Missing HRTIM specification for STM32H742/3

Hello,STM32H742/3 datasheet April 2021 DS12110 Rev 8 does not list a HRTIM specifications as e.g. STM32G474 datasheet DS12288 Rev 6 does in section  5.3.16 High-resolution timer (HRTIM). Please provide the data. Best regards 

Resolved! STM32h573 read OTP

Hello,I'm trying to read the OTP flash form my application but I get a hardfault.Is there a read protection or something like that? Here is a code snippet:#define FLASH_START_ADDRESS 0x08FFF000 int main(void) { HAL_Init(); uint32_t* flash_da...

CHeck.1 by Associate II
  • 4264 Views
  • 5 replies
  • 1 kudos

EEPROM in STM32H7 series

Hi, Greetings.Could you kindly confirm whether STM32 H5 and STM32H7 series have inbuilt EEPROM availability?From the datasheets of these series, I could not find EEPROM functionality specifically mentioned.Kindly confirm if there is an efficient alte...

STM32L496ZG MPU test

Hello, I'm trying to implement a MPU test on a STM32L496ZG MCU that will be part of some self-tests in our application. The MPU is working as expected and an interrupt occurs when I try to write to a protected memory region. But now I need to "catch"...

JBiVTSU by Associate
  • 923 Views
  • 0 replies
  • 0 kudos

Resolved! RESET PROBLEMS WITH STM32G474RET6

HelloI am new with using STM MCU's (STM32G474RET6) and encounter very strange reset behavior.In my application reset of the MCU can be done in 3 different ways. 1. Hardware reset - by pressing on button.2. Software reset - by executing NVIC_SystemRes...

error code-38 when starting FD-CAN

Hi,I'm trying to transmit some data using FD-CAN but HAL_FDCAN_Start() function returns error code 38. I have taken reference from STM32H743-EVAL kit example.I have configured same as mentioned there. But still i couldn't figure out the issue behind...

VPras by Associate II
  • 2788 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.