2023-12-12 2:28 AM
Hello,
I'm using a STM32L552CCT6. For firmware update I want to use the dual flash bank functionality of the controller.
When switching the flash banks with the option bit SWAP_BANK in register FLASH_OPTR what happens to the program counter? Is he also switched to the now second bank to continue the execution of the firmware?
Best regards,
Markus
Solved! Go to Solution.
2023-12-12 2:40 AM
The PC isn't changed.
The address decoder into the FLASH array fetches whatever maps to the address you requested
If the two banks have the same data underneath at the current point of execution you can basically fork()
2023-12-12 2:40 AM
The PC isn't changed.
The address decoder into the FLASH array fetches whatever maps to the address you requested
If the two banks have the same data underneath at the current point of execution you can basically fork()
2023-12-12 2:47 AM - edited 2023-12-12 4:26 AM
Thank you for your fast response :thumbs_up:.
So in my case:
When I run from bank 1, write a updated firmware to bank 2 and make a bank swap then the new firmware on bank 2 is executed immediately from that address to which the program counter is pointing at that moment, isn't it?
Best regards,
Markus
2023-12-12 5:03 AM - edited 2023-12-12 5:04 AM
Hello @dost
When switching the flash banks with the option bit SWAP_BANK in register FLASH_OPTR, the address mapping of user flash memory of each bank are swapped. Program counter should be always started executing from bank 1 (0x0800 0000). It is mentioned in Knowledge base article even though the context is different (H7 product).
How to configure swap bank on STM32H7 P2 - STMicroelectronics Community
Recommendation to take a look at limitations in errata for example to avoid reading from Bank 2 while writing in it. See ES0448 2.2.10 concurrent read from Bank 2 while erasing it as consequence of decreasing RDP level may result in unpredictable behavior.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.