2023-12-12 12:59 AM
Hello,
I'm trying to implement a MPU test on a STM32L496ZG MCU that will be part of some self-tests in our application.
The MPU is working as expected and an interrupt occurs when I try to write to a protected memory region. But now I need to "catch" this interrupt and continue the code execution like nothing happened.
I know I can override the MemManage_Handler and do some stuff in it but my issue is that when I return from the handler, it immediately enters again.
Is there any way I can exit MemManage_Handler and continue code execution normally ?
Here's my code:
int main(void)
{
// HAL init + clock init...
// Enable MemManage_Handler
SCB->SHCSR |= SCB_SHCSR_MEMFAULTENA_Msk;
// Configure MPU
HAL_MPU_Disable();
MPU_Region_InitTypeDef mpu_struct;
mpu_struct.Enable = MPU_REGION_ENABLE;
mpu_struct.BaseAddress = 0x081FF000;
mpu_struct.Size = MPU_REGION_SIZE_4KB;
mpu_struct.AccessPermission = MPU_REGION_PRIV_RO;
mpu_struct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
mpu_struct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
mpu_struct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
mpu_struct.Number = MPU_REGION_NUMBER0;
mpu_struct.TypeExtField = MPU_TEX_LEVEL0;
mpu_struct.SubRegionDisable = 0x00;
mpu_struct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
HAL_MPU_ConfigRegion(&mpu_struct);
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
// Test
uint32_t* p_write_addr = reinterpret_cast<uint32_t*>(0x081FF000);
*p_write_addr = 0xBADC0DE;
while (1)
{
HAL_GPIO_TogglePin(DO_LED_GPIO_Port, DO_LED_Pin);
HAL_Delay(1000);
}
}
Thanks !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.