STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SRAM3 Hard Fault when ECC is enabled

on STM32U575 when I enable the ECC, it is throwing a Hard Fault. I am just doing RAMCFG_Init() & StartECC() as of now. The system keeps resetting. TrustZone is enabled for the project, will that make any difference?

STM32G0: I2C Passthrough Implementation between i2c1 and i2c2

Hello,I need to implement an i2c passthrough between i2c ports i2c1 and i2c2 on my stm32g031k8 board. This MCU is connected to another CPU board using i2c2 port. Also, the i2c1 is connected to a temperature sensor, RTC,  and EEPROM. After power UP, u...

smoha.2 by Associate II
  • 2256 Views
  • 2 replies
  • 1 kudos

STM32F030 RTC - What happened to the Periodic Wakeup?

The original (Rev 1) datasheet said that STM32F030x4, x6, and x8 all had the Periodic Wakeup:The current (Rev 5) datasheet, which adds the xC variant, now says that only the xC has the Periodic Wakeup:So what happened?How/why did it disappear from th...

AndrewNeil_0-1702467536614.png AndrewNeil_1-1702467986690.png AndrewNeil_2-1702468304669.png

STM32F205RCT7 MTBF

Hi,I am doing the MTBF calculation of our product which contains STM32F205RCT7. Can you provide me with the MTBF value of STM32F205RCT7?Thanks in advance

YsnKcl by Associate
  • 1889 Views
  • 3 replies
  • 0 kudos

Hard fault caused by unaligned access

Hi, I have an issue when trying to copy a struct by direct assignment on STM32H743; The code:   void function(const structName_t *incomingStruct) { Signal_t sendSignal; sendSignal.desiredStruct = *incomingStruct; // <-- Causes unaligned access .....

RBrec.1 by Associate III
  • 20040 Views
  • 23 replies
  • 4 kudos

STM32U5 LL example ADC1 and ADC4

The example project does not provide information on ADC4 register configurations, ADC4 seems to be different then prior peripherals (e.g. compared to L4).  ...\NUCLEO-U575ZI-Q\Examples_LL\ADC\ADC_SingleConversion_TriggerSW_IT_InitSTM32CubeMX configur...

edw by Associate
  • 2696 Views
  • 0 replies
  • 1 kudos

spi slave weird data on mid-high speeds ?!

I am having weird issue with STM32F767 (configured to run at 200mhz) that needs to be SPI slave .. I configured it with 0,1 (clock low, second edge), hardware cs.. when master sends data at 350kbps everything is ok, when master sends at higher speeds...

arhi by Associate III
  • 10307 Views
  • 24 replies
  • 1 kudos

Can VDDA VREF+ and VssA connect to VSS(ground)?

I am using STM32H735,TFBGA-100 controller with 550MHz.I don't need ADC and DAC functions.1.Shall i connect VDDA,VREF+ and VssA to ground(Vss)? if yes, what is the recommended(through any resistor or  shorted)way to connect to Vss?2.If i did as above,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.