STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Weird Jitter when using DMA to generate PWM in GPIOs

So i was trying to generate pwm on all gpio pins of a stm32F103 for my application. I found followed this guide:https://www.hackster.io/javier-munoz-saez/all-pins-as-pwm-at-the-same-time-baremetal-stm32-1df86f the essence is using the function:      ...

Okbit_0-1702369391874.png Okbit_1-1702369391855.png Okbit_2-1702369391867.png
Okbit by Associate II
  • 3026 Views
  • 4 replies
  • 3 kudos

STM32L552 Azure RTOS ThreadX UART RX+TX not working correctly

Hi together,at work I have an Azure RTOS based project with UART communication. The basic implementation of ThreadX is working fine for toggling LEDs, but I need to do some SPI communication to an ePaper display and communicate with the MCU over UART...

BViet1_0-1701950414458.png
BViet.1 by Associate III
  • 4503 Views
  • 2 replies
  • 0 kudos

Resolved! Configure ADC sampling frequency STM32H723ZG

Hi All,I am using a STM32H723ZG Nucleo board. I am using the ADC in 8-bit mode. The clock is set to 96 MHz, and according to the application note it should use 6 cycles to sample and convert which would result in 16 Msps, but it seems to be between 8...

elso_0-1702459071410.png
elso by Senior
  • 1862 Views
  • 1 replies
  • 1 kudos

Resolved! can bus ack signal

I want to scan (acquire) data from a vehicle can bus.1. Is it possible to prevent the ACK bit from occurring in CAN communication in the MCU?2. If I set the ID to receive all data, won't an ack occur?

YPark.5 by Associate II
  • 4157 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H747 ADC Channels

I’m wondering which if these microcontrollers (STM32H7) has the most ADC Channels.I think the maximum is 36 but I want to know the specific model of MCU that this is, if anyone knows please tell me.I would also like to know if this is still a 16bit r...

MiltonR by Associate
  • 1892 Views
  • 2 replies
  • 0 kudos

Resolved! Handling of more than one external stldr loaders

Hi guys,so we have a more complex board and I wondered if it is somehow possible to use more than one external loaders with the CubeProgrammer software on the command line.So in general we are capable of writing these loaders and have several already...

Disabling JTAG

What are the different ways of disabling the JTAG in STM32G4 series? Is Direct Register Programming an option? 

Tushar_4 by Associate II
  • 3952 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.