STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U545RE USART3 issue

HelloI am using STM32U545RE (LQFP64 package) for my project as master controller. I am using the following pins for USART3 along with a transceiver chip ADM3061E and an additional GPIO output configured to act as the Enable.USART3_RX:PC5USART3_TX:PC4...

Roshan_Anand_0-1703877183772.png

Resolved! Optimizing DFT for loop

Do you think that it is common for the function bellow (arraySize = 32) to take approximately 125us to execute? The for loop is the main problem as it takes almost 120us to execute.I am using STM32G474ret6u MCU, with clock at 170Mhz? Also the optimiz...

GHrib.1 by Associate III
  • 2819 Views
  • 4 replies
  • 2 kudos

Resolved! STM32H7A3 LPUART and BDMA

I'm trying to get the LPUART working with BDMA on a STM32H7A3 MCU.  Eventually I'd like to set it up so the MCU goes into a low power state and wakes up when it receives a LF character match in the incoming message, but for now I'm just trying to get...

magene by Senior II
  • 7902 Views
  • 6 replies
  • 2 kudos

STM32 HAL or LL functions without the timebase

Hi All, I am using the STM32H723 device and have used the HAL functions and they work but I find the SysTick or any timebase interrupts my code. Timing is critical; if the data from the serial port is interrupted by the SysTick interrupt, I lose data...

ENort.1 by Associate III
  • 2018 Views
  • 2 replies
  • 1 kudos

LL_USART receive interrupt STM32G070 not working

Hi, Alli'm using stm32G070CBT6, i have some problem with low layer usart interrupt.the MCU seems always hang when received usart byte. Has anyone here experienced something similar?how to solved this case. thanks

Resolved! TIM2 on STM32F103RB board - how to set it up?

Hi, I have use MX to generate code for this timer.  The generated code is as follows: static void MX_TIM2_Init(void){ /* USER CODE BEGIN TIM2_Init 0 */ /* USER CODE END TIM2_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0};TIM_MasterConfigTy...

Resolved! How to set up IRAM1/IRAM2 in Keil with STM32H742VIT6?

Hello,I'm having weird problems with code crashing, perhaps related to how I have IRAM1/IRAM2 set up in my project:Looking in the reference manual, I see that the SRAM starting at 0x2000_0000 is the DTCM_RAM on TCM interface (data RAM?), the SRAM sta...

briankaz_1-1703032836804.png
briankaz by Associate III
  • 11655 Views
  • 17 replies
  • 2 kudos

Resolved! DAC output offset spec with output buffer enabled

Hi,Currently, we are facing an accuracy problem when using the built-in DAC on the STM32F407 (with buffer enabled). As the built-in reference voltage measured 2.0005V, we set the DOR to 0x800, expecting to get 1.25V on the DAC output. However, we act...

calvin by Associate III
  • 11076 Views
  • 11 replies
  • 4 kudos

Resolved! Questions about G474 FDCAN

The FDCAN loopback test of G474 can enter the receive interrupt, but normally the two devices communicate with each other, and when one of the devices is used to debug, it is found that the interrupt cannot be entered。  

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.