2023-12-29 11:11 AM - edited 2023-12-29 11:14 AM
Hello
I am using STM32U545RE (LQFP64 package) for my project as master controller. I am using the following pins for USART3 along with a transceiver chip ADM3061E
and an additional GPIO output configured to act as the Enable.
USART3_RX:PC5
USART3_TX:PC4
Enable:PB1
But on transmitting the data I am not getting any data on the output A,B pns(as in diagram).
But the same works with STM32L496RE uC, may I know what is the cause of this problem here?
On referring to the STM32U545xx Errata sheet, we got to know that the device that I use also has Z marking.
Is there a workaround available if the above problem is because of the untrimmed uC samples?
Regards
Roshan Anand
2023-12-29 1:54 PM
What specific issue in the Errata are you worried about? https://www.st.com/resource/en/errata_sheet/es0587-stm32u535xx-and-stm32u545xx-device-errata-stmicroelectronics.pdf
Put a pull-up on the RX pin, or enable internally.
Double check RCC clocks for GPIO and USART3. Check USART3 registers. Check HSE_VALUE
Check that the USART isn't flagging any sticky error that needs to be cleared.
Do you see data on the TX pin? Which pins?
SHOW CODE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.