2018-09-12 9:41 AM
Hello Folks!
So far, I've been able to utilize the FSMC/FMC peripheral in many different scenarios, including interfacing LCDs in 8080 mode, legacy ASICs, SDRAMs, etc. I'm now working on a project that involves M29EW Parallel NOR Flash (1GB single-die TSOP) and I was wondering if the FMC (STMF429) can address 1 GB of continuous memory space. As far as I know, BANK 1 of the FMC that is dedicated for the NOR-type of memory is divided across 4 sub banks with an individual chip-select (NE) for each bank. With that being said, if I have configured the FMC for 26 address bits on a given NE, would it be possible then to address a 1-GBit (128 MBytes) of continuous memory space?
Thanks,
Zaher
2018-09-13 12:04 PM
M29EW_CE = FSMC_NE1 & FSMC_NE2
M29EW_A25 = FSMC_NE1
M29EW_A[0..24] = FSMC_A[0..24] - ARM_A[1..25]
M29EW_D[0..15] = FSMC_D[0..15]
Plus whatever you need to do with read, write and byte lanes, etc
2018-09-13 2:45 PM
Thank you very much for the detailed and very helpful input. The part # is: JS28F00AM29EWLA. I have attached the datasheet for reference at will.
Yes, I was thinking about doing some experimentation on the STM32F429 board level by monitoring the state of the FMC pins during bus transactions. However, I do not have the flash connected to the board at the moment, so I'm not sure if I can do the job right now without connecting an actual memory to the FMC peripheral. I guess some timing and signal feedback rules apply here. Not sure if that can work out without an actual memory device.
Thank you again for your excellent support!
2018-09-17 5:11 PM
By the way, since NE2 has to be enabled in the CubeMX configurations, I think I must have two separate setup and access functions for each handle. This is another limitation, but I guess it's not difficult to write some functions to get things automated for read/write access on both banks in the 128MB space.
I'm almost done on the PCB. I should have a prototype with an exposed header so I can change the wiring between the STM32F429 and the M29EWL at will.
2018-09-17 6:08 PM
Like I said earlier, the decode banks are 64MB wide, you need to AND NE1 with NE2
2018-09-18 3:18 AM
This could've been quickly tried also with a Nucleo-type board with a small SRAM such as 6264/62256 or a small 29Fxxx FLASH (or, for that matter, a 27xx EPROM or 28xx EEPROM) wired up to the highermost addresses.
JW
2018-09-29 12:42 PM
Well, I wanted to give it a try on an actual 1 Gbit M29EWL so I have designed and ordered the PCB for this purpose. I made it with a pin header so I can exchange signals at will between this prototype PCB and the STM32F4 board. I will report my testing over here once done!
Thank you guys!
2018-10-03 1:43 AM
Again, access to the second 64 MB (sub-bank 2) fires a Hard Fault interrupt if NE2 was not enabled initially. This is also mentioned in the RM of the device. With that being said, there will be a separate hnor handle for configuring/accessing the memory for each individual sub-bank. I guess I will have to write a function in such a way that switches between handles/sub-banks accordingly. Please correct me if I was wrong or if you think there's a better way to do it.
2018-10-03 3:49 PM
> access to the second 64 MB (sub-bank 2) fires a Hard Fault interrupt if NE2 was not enabled initially
Simply enable both sub-banks and with the "address reconstruction" and merging the chipselects (NEx) you should be able to access a continuous 128MB space.
JW
2019-11-13 6:00 AM
Hi guys,
Thank you very much for your information, could you please tell me more detail about "the "address reconstruction" and merging the chip selects (NEx)" as you mentioned?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.