cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303 maximum ADC sampling rate

Mercadei
Associate

Hi everyone,

I am currently looking into the STM32F303CCT6 and I'm a bit confused by the ADC specifications. ST's website mentions it can achieve up to 18 MSPS in interleaved mode. However, looking through the Datasheet and the Reference Manual (RM0316), I don't see a clear way to hit 18 MSPS at 12-bit resolution.

I realize the hardware interleaved mode is only dual (e.g., ADC1/2 and ADC3/4). Since the documentation mentions dual mode can reach up to 9 MSPS at 12-bit, and there is no native quad-interleaved mode, I suspect one of two things:

  1. There is a way to manually coordinate the two dual pairs (using all 4 ADCs) to reach 18 MSPS at 12-bit.

  2. The 18 MSPS claim strictly refers to running a dual interleaved setup at a reduced 6-bit resolution.

I would deeple appreciate some insight regarding if 18 MSPS at 12-bit is actually possible on this MCU, or if I am limited to the dual mode specs?

Thanks in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Super User

Hi,

as @mƎALLEm explained, no "quadruple mode" .

 

But you could try: 

- set all 4 ADC to max. speed settings (sampling time, one ch conversion), on trigger mode

- set TIM1 to 144 MHz ; use 4 signals (TRG, TRG2 ; compare 2 , 3 ) as start/trigger for the 4 adcs

- set for all adc DMA channels

- now , set/separate the delays to equal values, so starting the timer giving a sequence of triggers 

Should work, to get a combined sample rate of 18 Msps.

With little overclocking:

At 80M core, 160M on TIM1 , ( arr 32 ) with 8 ticks spacing between triggers, could reach 20 Ms.

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello @Mercadei and welcome to the ST community.

There is no “Quadruple” mode available. Only Dual mode. Where:
ADC1 is a master and ADC2 is its slave. 

ADC3 is a master and ADC4 is its slave.

Not possible to synchronise all the ADCs as in quadruple mode. So not possible to reach 18MSPS at 12 bit resolution.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
AScha.3
Super User

Hi,

as @mƎALLEm explained, no "quadruple mode" .

 

But you could try: 

- set all 4 ADC to max. speed settings (sampling time, one ch conversion), on trigger mode

- set TIM1 to 144 MHz ; use 4 signals (TRG, TRG2 ; compare 2 , 3 ) as start/trigger for the 4 adcs

- set for all adc DMA channels

- now , set/separate the delays to equal values, so starting the timer giving a sequence of triggers 

Should work, to get a combined sample rate of 18 Msps.

With little overclocking:

At 80M core, 160M on TIM1 , ( arr 32 ) with 8 ticks spacing between triggers, could reach 20 Ms.

 

If you feel a post has answered your question, please click "Accept as Solution".

Hello all,

Thank you both for your answers, and apologies for the delayed response, I wanted to test the HW before getting back to you.

After a couple tests with the NUCLEO-F303RE DK, I managed to achieve a clean and stable 18 MSPS at 12-bit resolution by synchronizing the four ADCs independently (just as @AScha.3 said).

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.