2025-01-31 1:23 AM - last edited on 2025-01-31 4:11 AM by Andrew Neil
Created a new thread from STDRIVE101 PWM Output Jitter Inquiry here because it is a question about a completely different device.
Dear Peter,
Thank you for your explanation. That clarifies the behavior of the STDRIVE101.
I have two follow-up questions:
I appreciate your insights.
Best regards,
Aji
Solved! Go to Solution.
2025-01-31 6:15 AM
Regards
/Peter
2025-01-31 3:45 AM
Regards
/Peter
2025-01-31 4:21 AM - edited 2025-01-31 4:21 AM
Dear Peter,
Thank you for your response. I’d like to clarify my questions further:
The STSPIN32G4 consists of an STM32G431 and a motor driver. My question specifically concerns the motor driver section. For example, if the PWM generated by the STM32G431 timer has no jitter at all, would the output from the motor driver also be completely jitter-free?
My question is about the motor driver itself, not the MCU. Some motor driver ICs from other manufacturers include an internal clock, which can introduce jitter in the output. Does the motor driver section of the STSPIN32G4 have an internal clock that could affect the output in a similar way?
Best regards,
Aji
2025-01-31 6:15 AM
Regards
/Peter
2025-01-31 10:35 AM
Hi Peter,
No, that level of jitter is already small enough and does not pose any issue. Thank you for addressing my concerns so clearly. I really appreciate your detailed explanation.
Best regards,
Aji
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.