2020-04-26 11:25 AM
I am having a devil of a time loading an existing MC_SDK project using STM32Cube. When I try to load an existing project potentiometer.ioc I get an error "Can't Add: Motor Control files not found". Does ST32Cube not see MC_SDK?
To be more specific I launched ST32CubeMx and loaded Potentiometer.ioc from the install folder C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.4.3\Projects\P-NUCLEO-IHM001\Demonstration\Potentiometer
I installed ST32Cube first and ran it several times before installing MC_SDK. Both were installed using installer and default folder locations.
2021-06-14 11:34 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.