2020-01-16 5:49 PM
After Workbench and Keil firmware was doenloaded to STM32F103RC. But it showed Unkown error when I tried to run the motor via Worknench. When stop run button was clicked it show "any stop". Anyone can tell me what happened and what should I do? Thank You
2021-06-14 11:37 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.