2024-03-22 10:09 AM - edited 2024-03-22 10:10 AM
I am essentially experiencing the exact same issue as this poster.
I have a single conversion registered, on ADC1 channel 13. It works great for ages, and then the RCM_execRegularConv function gets "stuck" waiting for end of conversion.
I am running MC workbench 6.1.2 - unlike the poster in the link, I did not declare the handle on the stack, and it does not appear to be getting corrupted - I can stop the program and see that the reference to the ADC is still intact. I am trying to reproduce again, so I can look at the registers on the ADC that reflect the state of conversion, but this really is a *rare* issue, so it's difficult to reproduce it quickly for testing.
-R
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.