STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

FOC Phase Current Noise (Low Inductance Motor)

Greetings,The motor I am working on is low inductant ~0.1mH with a max speed of ~2500rpm. I am wrestling with noise on the measured phase current signals, which distorts the control loop and in the end results in bad control or 'Over Current' Fault. ...

Sensorless_startup_torque_075A_v1.png Sensorless_startup_torque_075A_v1_scope.png

Regular Conversion Manager Hang on EOC

I am essentially experiencing the exact same issue as this poster.  I have a single conversion registered, on ADC1 channel 13. It works great for ages, and then the RCM_execRegularConv function gets "stuck" waiting for end of conversion.   I am runni...

MCSDK debug error

Hi,Im currently tring to program my nucleo-f103rb module. I have succesfully generated Motor control workbench project and CubeMx project. After code generation using cubemx , stm32cubeide1.8.0 opens the project code. Without changing anyting on the ...

qqwq.1 by Associate II
  • 3721 Views
  • 7 replies
  • 0 kudos

Resolved! B-G473E-ZEST1S UM3118

Where to find user manual UM3118 referenced in B-G473E-ZEST1S Data Brief.The link to this manual in the data brief goes to Page Not Found.Many thanks.

elgeeds by Associate
  • 4451 Views
  • 2 replies
  • 0 kudos

Motor profiler - BLDC

I am trying to identify the motor parameters of a BLDC (with a multipolar magnet rotor) using Motor Profiler. Should I select SM-PMSM or I-PMSM in magnetic built-in?Thank you in advance for your answer. King regards,Cristhian Chavez Thank you in adva...

motor_prof.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.