2020-07-09 5:26 AM
im very new with EVALKIT-ROBOT-1. I loaded the EVALKIT-ROBOT-1.stmx V5.4.3 File which was delivered with the Kit into the MCWB 5.4.3. Because in can’t find a Board named STEVAL-SPIN3201 i can’t use the MotorProfiler.
When i load the EVALKIT-ROBOT-1.stmx V5.4.3 into the MCWB 5.4.3. and open the Monitor i can’t Connect to the Device. I tried all Baudrates and used the Com45 who i got new, when my RS485-Adapter was connected on USB.
I tried that first with the original Firmware delivered on the EVALKIT-ROBOT-1. I generated a new *.ioc File with the settings STM32CubeMX 5.6.1 and the Toolchain ST STM32CubeIDE and selected the STM32 FW V1.11.0 Firmware-Package (Recommended). I selected the LL-Driver-Type.
I compiled the Project Error-Free and programmed the resulting EVALKIT-ROBOT-1.elf over the STMcubeProgrammer with StLink V3 to the EVALKIT. Verify was OK.
But with this firmware, there was also no Connection in MCWB-Monitor possible.
Questions: The Connetion runs over the RS485 Cable, not over the ST-Link ist hat Correct ?
Whas is going wrong?
2021-06-27 11:00 PM
Adding of "STM32 Motor Control" topic.
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.