2021-09-05 5:59 AM
Other setting provided with Motor Profiler
1. DC Connected 12 V adapter 1 A
2. Pole pair 7
3. Max Speed 12000 rpm
4. Max Current o.96 APK
Its working and profiler shows following results
a. Imax 0.9 Apk
b. Rs 0.51 ohm
c. Ls 0.03mH
d. VBus 11.6V
e. Ke 0.76 Vrms/kRPM
f. Friction 189.76 nN m s
g. Inertia nN-m-s2
h. Max Speed 11970 Rpm
2021-09-22 4:39 AM
Hi @GSrik.2 and welcome to the ST Community.
Since your question is about STM32 MCSDK, I added the topic "STM32 Motor Control", user of this community are experts of ST Workbench and can help you.
From hardware point of view, in addition to your list, check the following points:
When you use the external power supply (applied to J1 of X-NUCLEO-IHM07M1) it is still possible to use the USB for communication, but it is mandatory to power supply the MCU board first using VIN (through CN7-24 pin) then connect the USB cable to the PC.
The following power sequence procedure must be respected:
If I understood the motor profiler working correctly, but then you cannot run the motor.
Which example are you using?
With your board HW configuration you would like to implement a sensored FOC, right?
Moreover, can you share more details about your tools and versions (do not forget to also indicate the compilation tools suite you use?
2021-10-12 2:18 AM
Hi @GSrik.2 any updates about your project?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.