STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

STEVAL-IPMNG8Q-3h???

Hi,I have STEVAL-IPMNG8Q-3h and I want to drive PMSM motor.In the code generated by the ST WORKBENCH, I get this error!!"Description Resource Path Location Typeunknown type name 'RTC_HandleTypeDef'; did you mean 'I2C_HandleTypeDef'? stm32f3xx_hal_tim...

Eakso.2 by Associate II
  • 1949 Views
  • 4 replies
  • 0 kudos

Need higher resolution speed measurement in FOC code.

In my sensorless application driving a BLDC I need the best resolution possible. I set the SPEED_UNIT to _001Hz but the feedback from the SPD_GetAvrgMecSpeedUnit procedure still seems to be in units rounded to 6. For example I can read 3059 and 3064 ...

BTrem.1 by Senior II
  • 1699 Views
  • 3 replies
  • 0 kudos

MC Workbench cannot generate projects with CubeMX 6.3.0

Hi all,​I am using MC Workbench to generate motor projects.​As I upgrade my STM32CubeMX to 6.3.0, it doesn't work anymore.​I can directly use STM32CubeMX, but cannot generate source via MCWorkbench.​I tried MC Workbench 5.4.4, 5.4.6, 5.Y.1, and all o...

JHSU.16 by Associate
  • 2168 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.