2021-06-14 11:23 AM
Hi,
Is there any way to use Motor Profiler with EVSPIN32F601S3 Board ?
--
Karan
Solved! Go to Solution.
2021-06-15 12:25 AM
Hello Karan,
The EVSPIN32F0601S3 board is based on the STSPIN32F0601 controller which embeds a Cortex M0.
As Cortex M0 does not have FPU, Motor profiler can not be developed for this board.
Regards
Cedric
2021-06-15 12:25 AM
Hello Karan,
The EVSPIN32F0601S3 board is based on the STSPIN32F0601 controller which embeds a Cortex M0.
As Cortex M0 does not have FPU, Motor profiler can not be developed for this board.
Regards
Cedric
2021-06-15 12:32 AM
Thanks.. for update..OK ..
Any other board compatible with NUCLEO-F302R8 for High Voltage BLDC Development . supports Motor Profiler ?
Input voltage from 50 V to 280 V DC/AC
--
Karan
2021-06-15 12:39 AM
All available combinations control + power boards are showed in Motor profiler tool. Click on "select boards" button from the main window to have access to all of them.
Cedric
2021-06-15 12:40 AM
Ok.. Thanks ..
No Combinations for Input voltage from 50 V to 280 V DC/AC ?
--
Karan
2023-07-18 5:20 AM
Were you able get a solution on this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.