STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Help setting the comparator for the timer brake. Internal connection between the comp and TIM1 with complementary outputs

Hi, I'm setting up a custom board with STM32G431CBT6 to control a 6-step bldc motor. I want to use comparators to protect against overcurrent.My problem I configured the bkin input and comparators. the bkin input works, the comparator also works sepa...

_legacyfs_online_stmicro_images_0693W00000bid4IQAQ.png _legacyfs_online_stmicro_images_0693W00000bid4NQAQ.png _legacyfs_online_stmicro_images_0693W00000bid4SQAQ.png _legacyfs_online_stmicro_images_0693W00000bid4XQAQ.png
MGrod by Associate II
  • 2273 Views
  • 1 replies
  • 0 kudos

Resolved! STSPIN32G4 random gatedriver or timer1 output shutdown

Hello I am using a custom design with the STSPIN32G4. Running open loop space vektor commutation works, but after a random amount of time the motor simply stops.Surprising is that if SPI is active the error seems to occure sooner than normal. Everyth...

DWiec.1 by Associate
  • 2436 Views
  • 2 replies
  • 0 kudos

Lot of mistakes in MC SDK documentation

Large number of mistakes observed in the MCSDK documentation UM1052. This is the park transform and the same thing is repeating. Is he trying to say Ia, Ib or Ialpha or IBeta. I think very little effort in creating the document. There is a mention o...

0693W00000biARwQAM_image.png _legacyfs_online_stmicro_images_0693W00000biASBQA2.png
SRedd.5 by Senior III
  • 1280 Views
  • 2 replies
  • 0 kudos

We are working on a board with, among other things, TPS56637 and TPS62913RPUR voltage regulators, a couple of DRV8912-Q1 motor drivers, two ALM2402-Q1 op amps, and an analog subsystem measured by an STM32G474 MCU.

We are working on a board with, among other things, TPS56637 and TPS62913RPUR voltage regulators, a couple of DRV8912-Q1 motor drivers, two ALM2402-Q1 op amps, and an analog subsystem measured by an STM32G474 MCU. What type of separation of ground pl...

HZHAN.4 by Associate
  • 917 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.