2023-11-10 9:45 AM - edited 2023-11-10 9:50 AM
Hey everyone,
I'm currently enrolled in Electronics and Power Engineering major, and I'm super excited about my project to create a PMSM Motor Driver, which I'd utilize STM32 PMSM FOC SDK with the ST MC Workbench. I'll be interfacing the STM32F446 as the controller with a custom-made inverter (Power Driver).
Right now, I'm in the research phase to figure out the best Power Board components and parameters for my application. However, I've run into a little bump - when I open ST MC Workbench, it asks me to choose from defined power drivers. I actually want to use my own custom power driver that I'll build. Can anyone provide guidance on how I can use a custom power driver board with the ST MC Workbench? Also, are there any tips I should consider when choosing the components to work best with my STM board and/or ST MC Workbench?
I'd really appreciate any help or advice you can offer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.