2021-11-25 8:02 PM
I've designed an FOC board.First of all,I want to realize the SVPWM without using other transformation in order to make the motor rotate first.
PWMC_SetPhaseVoltage(pwmcHandle, Valphabeta);so I generate an array about Valphabeta as the code below:
#define PIDIV180 0.017453292519943
#define MAX 25000
int main()
{
double cnt=0,angle;
int a,b;
printf("int16_t test1[][2]=\n{\n");
for(cnt = 0;cnt<90;cnt+=0.05)
{
angle = cnt * PIDIV180;
a = MAX*cos(angle);
b = MAX*sin(angle);
printf("{%d,%d},\n",a,b);
}
printf("};");
return 0;
}and the FOC code is changed to below:
cnt = (cnt+1)%1800;
if(!cnt)
{
cnt1 = (cnt1+1)%4;
}
switch(cnt1)
{
case 0:// 4 quadrand
a = test1[cnt][0];
b = test1[cnt][1];
break;
case 1:// 3 quadrand
a = -test1[cnt][1];
b = test1[cnt][0];
break;
case 2:// 2 quadrand
a = -test1[cnt][0];
b = -test1[cnt][1];
break;
case 3:// 1 quadrand
a = test1[cnt][1];
b = -test1[cnt][0];
break;
}
Valphabeta.alpha = a;
Valphabeta.beta = b;
hCodeError = PWMC_SetPhaseVoltage(pwmcHandle, Valphabeta);when PWM_FREQUENCY is above 10k,the motor rotates,but when PWM_FREQUENCY is slow like 5k,the motor rotates back and forth at a small angle.
Where is the problem?FOC frequency can't be too low or my test method is wrong.
Solved! Go to Solution.
2021-11-27 7:08 AM
Solved.It depends on the ADV_TIM_CLK_MHz.
#define ADV_TIM_CLK_MHz 128
#define PWM_FREQUENCY 5000
#define PWM_PERIOD_CYCLES (uint16_t)((ADV_TIM_CLK_MHz*(uint32_t)1000000u/((uint32_t)(PWM_FREQUENCY)))&0xFFFE)
and the variable:
.hT_Sqrt3 = (PWM_PERIOD_CYCLES*SQRT3FACTOR)/16384u,
is out of bound.
2021-11-25 11:48 PM
The X-CUBE-MCSDK standard code works well at frequencies lower than 10kHz. The lowest supported PWM frequency is in fact 2kHz. The optimal PWM frequency depends on the motor parameters.
2021-11-27 7:08 AM
Solved.It depends on the ADV_TIM_CLK_MHz.
#define ADV_TIM_CLK_MHz 128
#define PWM_FREQUENCY 5000
#define PWM_PERIOD_CYCLES (uint16_t)((ADV_TIM_CLK_MHz*(uint32_t)1000000u/((uint32_t)(PWM_FREQUENCY)))&0xFFFE)
and the variable:
.hT_Sqrt3 = (PWM_PERIOD_CYCLES*SQRT3FACTOR)/16384u,
is out of bound.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.