STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Timers

Hi,So I presently have this problem. As seen in the picture, my timer1 time base is set to 1919 and it has a 48MHz clock source, which means I should produce signals with frequency of 25kHz. But this is not the case. instead the output signals from t...

0693W00000F9u8sQAB.png

Motor Control workbench

Hi, I am using NUCLEO-F303RE, I have purchased a power board (IPM evaluation board EVALM13645ATOBO1) from Digikey.In the Motor control workbench, I didn't find above mentioned power board part no. so, can you tell me, which one I need to select in th...

0693W00000DmMqMQAV.png 0693W00000DmMqCQAV.png 0693W00000DmN1UQAV.png

GPIO pin doesn't have output

I configure 6 channel GPIO pins to generate PWM signals to control 3-phase bridge. There is one pin(PC13) sometimes stop to generate signal. Even we reset 3.3V power voltage, it won't recover. one time I inject 20k square wave to pin PC13 to verif...

LFu.1 by Associate II
  • 1516 Views
  • 2 replies
  • 0 kudos

What cause MC_START_UP Failure with RUC_Exec routine?

I saw a problem posted 2 years ago similar to my problem now but the issue was closed with a ticket filed and I can't access any follow ups. Start-up failure, MC_START_UP fault flag getting set sometimes. Posted on April 12, 2018 at 23:49Using the M...

BTrem.1 by Senior II
  • 2999 Views
  • 3 replies
  • 0 kudos

Control Function.

Hi All,Can someone please enlighten me on this:Why is the integrator term, and the control function output scaled and shifted as shown in this code below?Why would I need to do that in an embedded system such as STM32?

0693W00000Dma3JQAR.png

ST motor control workbench connection failed!

I used STSPIN32F0A as my motor control chip, the X_CUBE_MC workbench version is 5.4.4 , and the firmware package version is ST32 FW v1.11.2, then I generate the code ,but when I connect the MC workbench , I couldn't connect the MC workbench seria...

0693W000007ERPdQAO.png
Wzong.1 by Associate III
  • 3041 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.