STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

What to change to make speed keep up under load?

I'd like to make our application more aggressive so that it can keep its speed constant under different loads.The speed regulator seems to be dialled in pretty good as it follows our setpoint perfectly fine.However, when I load the motor, the current...

DMeie.2 by Senior II
  • 2581 Views
  • 5 replies
  • 2 kudos

X-CUBE-MCSDK V.6.3.1 has no BLDC motor selection

 Hi,I am currently working on a research and development project for a Dual Inverter Air Conditioner, where I need to run a BLDC motor for the compressor in the outdoor unit.I have installed the X-CUBE-MCSDK version 6.3.1 and started exploring its fe...

NamZC14 by Associate
  • 2084 Views
  • 1 replies
  • 0 kudos

Code deleted after re-generation

I generated with MC Workbench some code sa use to program an inverter. I want to plot with the monitor the value read from the potentiometer, i.e., the value stored in "rawValue"I had managed to graphically plot on the monitor "rawValue" variable use...

luke514_0-1729863051366.png
luke514 by Senior
  • 1815 Views
  • 3 replies
  • 2 kudos

Resolved! How to set a glitch free 100% duty cycle PWM output

To control a DC motor driver I need to set one pin permanently high and the other is inverse PWM.If I want to reverse the motor direction I need to swap these settings.So I configured both pins as PWM output.But if I want to set one output pin high t...

WSpar.1 by Associate III
  • 5313 Views
  • 3 replies
  • 2 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

How to calculate the Ke?

I refer here:https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32MotorControl:How_To_manually_configure_the_motor_parameters Below is the profiler's result. Ke=9.59 Vrms/kRPM.Below is my owm test.Vpp=13.6v,pole pairs=5,fbemf=83.33Hz. Ke=(13.6*5*100...

Setup_motor_parameters_manually-7.png 20231008160258.png TEK00107.PNG
gtop.1 by Associate III
  • 6343 Views
  • 9 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.