2024-10-18 3:31 AM - last edited on 2024-10-29 7:01 AM by Andrew Neil
Hi,
I am currently working on a research and development project for a Dual Inverter Air Conditioner, where I need to run a BLDC motor for the compressor in the outdoor unit.
I have installed the X-CUBE-MCSDK version 6.3.1 and started exploring its features. However, I noticed that in the motor selection section, there are only 11 motor options, all of which are for PMSM motors.
I am a bit confused as to whether I can operate a BLDC motor using this software and if any of the available PMSM motor options can be adapted to run a BLDC motor. Could you please advise on how to proceed with this, or if there are any necessary modifications I should make?
Thank you for your support.
2024-10-29 6:51 AM
Hello NamZC14,
Did you have a look at this post ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.