STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Read only from one channel of the ADC

I have two active ADCs with many channels reading, some in regular converison, some injected, etc.The code is autogenerated from MC Workbench, but I added a channel 11 for an external potentiometer.I don't really know in the autogenerated files where...

luke514_0-1729697663038.png luke514_0-1729698295963.png
luke514 by Senior
  • 2280 Views
  • 4 replies
  • 0 kudos

Increasing Current for a BLDC Motor Under Load

Hello ST Community,I'm using an X-NUCLEO-IHM17M1 shield with a NUCLEO-F401RE board to control a 6V BLDC motor (motor specifications are attached below). Both the 6-step and FOC control algorithms are functioning as expected, and the motor operates co...

hashiR_0-1729920343811.png
hashiR by Associate III
  • 1013 Views
  • 0 replies
  • 0 kudos

Motor Commands to preserve pre power operation?

Hello.I am running an x-nucleo-IHM03A1 with a Nucleo-F401RE and a 24BK20-30 Stepper motor.  I have FW that allows me to push a button to arm the device and then 2 other buttons that allow me to run the device using the MOV command to create upper and...

SWenn.1 by Senior III
  • 885 Views
  • 0 replies
  • 0 kudos

Resolved! HSO PI tuning with MCSDK 6.3.1

Hello, I am getting up and running with the STM32 ZeST Kit to evaluate the HSO capability. Components: 1) STEVAL-LVLP012) B-MOTOR-PMSMA13) B-G473E-ZEST1SI am currently on MDSDK 6.3.1, and Motor Pilot V1.2.11 (MC_FOC_ZEST). I was able to successfully ...

rms_st by Associate II
  • 2143 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.