STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Can't reach application speed

MCSDK Version is 6.2.1.I'm currently having the issue that our motor doesn't reach the configured application speed of 7600RPM.It stops increasing in speed at around 6500RPM.The motor is slightly loaded for my tests. I'm running in Torque mode with t...

DMeie.2 by Senior II
  • 1376 Views
  • 2 replies
  • 0 kudos

EVSPIN32G4 with MCSDK 6.3.2

Hey, I had recently purchased an EVSPIN32G4 board, and I'm currently trying to use the MCSDK to generate code for it.When I'm trying to generate code for it, it completes with the following error:How can I solve this issue?Thanks,Eyal

Ek92_0-1732018370359.png
Ek92 by Associate
  • 872 Views
  • 1 replies
  • 0 kudos

Changing desired torque at run time

Dear all,I have a NUCLEO-F302R8 and the X-NUCLEO-IHM07M1 motor driver expansion board. I have a three phase BLDC motor with an encoder attached to it. I want to implement a torque controller. I am able to use the workbench software to implement the t...

nonameX_0-1709053114559.png
nonameX by Associate
  • 2381 Views
  • 4 replies
  • 0 kudos

Resolved! Regular Conversion Manager Crashing

Hi, I'm using MCSDK 5.Y.2 and STSPIN32G4 on a custom board. (this is a software thing !)I couldn't find a way to get two (more than one) converted ADC Values using a single request using the RCM.So I carried on converting each channel sequentially.I ...

Muthanna by Associate III
  • 3733 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.