STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

STSPIN32G4 EMI radiation problem

Hello I need help for STSPIN32G4 EMI IssueI took tests for Farfield EMI Report at STSPIN32G4 Standby conditionReport shows QP are over than Limit at 189 MHz, 252MHz.  It doesnt depend on the input voltage and the signal  peeks are visible also if the...

jopa_0-1732780186721.png
jopa by Associate
  • 873 Views
  • 0 replies
  • 0 kudos

Nucleo-G071 and EVSPIN958. How to?

Is there any support for evspin958 connected to the Nucleo-G071 board? I’m not really sure how to proceed. I need to control a DC motor back and forth using PWM. I can’t find any libraries. X-CUBE-MCSDK doesn’t seem to support this combination. STSPI...

Nalle by Associate
  • 715 Views
  • 0 replies
  • 0 kudos

Resolved! Firmware request for UM2647 product

Hi,   I am interested in the um2647 product. Like to explore more in 6step firmware, how to download the firmware for this product. I saw that using work bench it can be extracted, but I need the complete code which cannot be done in the work bench.

Bud by Associate III
  • 1256 Views
  • 1 replies
  • 0 kudos

FOC steps in code in NUCLEO-IHM07M1

Sorry for any silly questions asked, but please help since I am actually a beginner.Ques: I can see most of the FOC steps are inside "FOC_CurrControllerM1" function. And we just add below code in main() for motor to start and run: MC_ProgramSpeedRamp...

Resolved! Position Control using Hall Sensor

Hi, I'm newbie to Motor Control workbench(6.3.2) . I have STM32 G431RB and IHM08M1.I want to control the position of BLDC (42BLFX01E). This motor has 3 Hall Sensors.  I successfully run the motor using motor profiler and implemented the speed control...

Screenshot 2024-11-25 121016.png
SannanAli by Associate II
  • 2041 Views
  • 1 replies
  • 0 kudos

Resolved! Cannot choose HallEffectSensor

I'm trying to set up a custom board based on the B-G431-ESC1, with the MC Workbench and the SDK Version 6.2.1.My intention is to use sensorless for development and then have the option to switch to sensored (Hall, Encoder) in the future.I set up the ...

DMeie.2 by Senior II
  • 2857 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.