STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

X-NUCLEO-IHM08M1 Dead Time

Hello everyone,I am utilizing the IHM08M1 board for a Voltage Source Converter (VSC) academic project.The IHM08M1 board's Gate Driver L6398 already incorporates a set deadtime of 320 ns for the control signals of LVG and HVG.I would like to know if t...

Resolved! How to increase Phase Voltage?

MCSDK version is 6.2.1Our motor is running fine and can drive some load, however I'd like to increase the Phase Voltage with which our motor is driven to further increase its power output.When checking the High Frequency Plot for V_Q (and thus the pe...

DMeie.2 by Senior II
  • 1878 Views
  • 2 replies
  • 1 kudos

Issue in running motor using custom board STSPIN32F0

Dear, I have custom board based on this https://github.com/issus/BLDC-Drive which uses STSPIN32F0 as motor driver. I have that got that PCB manufactured & assembled but stumbled on an issue (which I assume is an issue) that it does not have feedback ...

x4ce by Associate III
  • 1892 Views
  • 2 replies
  • 0 kudos

B-G431B-ESC1 with FOC

I am trying to run an A2212 13T motor with B-G431B-ESC1 motor with FOC algorithm.But the motor gets stopped after attaining a low speed.Solve the problem.

Resolved! Custom Board bringup issues

[VERSION]: 6.3.1[TOOL]: Board Designer, Motor Pilot, MCSDK[DETAILS]: Created custom board based on IHM16M dev kit, using STM32G431RB + DRV8323. Motor Pilot cannot spin motor, but encoder signals look accurate, Vbus signal is accurate, and current sen...

shanemattner_0-1731091672956.png shanemattner_1-1731091696880.png shanemattner_2-1731091711399.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.