STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

B-G431-ESC1 Board: ST890 issue

As my understanding, ST890 used for isolate USB 5V and Battery 5V( DC/DC from 10V by U12: LDFPVR ). And also provide 5V for ESC board in debug program even  without battery connected.But why when I use battery only, which means no usb pluged, there i...

Kai123_0-1736517262389.png
Kai123 by Associate
  • 710 Views
  • 0 replies
  • 0 kudos

How to use nucleo-IHM08M1 on nucleo stm32f767

Hey I was I wondering if it was possible to use the x-nucleo-ihm08m1 on an 144 board.I only have 144 pin boards but couldnt find my board on MC Workbench.I also tried the motor pilot software and it said to configure the board.I suppose I can use it ...

Where can I find HW deadtime setting?

We're using a driver that inserts a deadtime by hardware.It is not clear to me how I have to configure that into the MCWB firmware to get ADC measurement working properly.I see three deadtime-related settings:- "minDeadTime" property in the "PhaseVol...

DMeie.2 by Senior II
  • 2187 Views
  • 3 replies
  • 1 kudos

Startup failure at load

I profiled my motor using the Profiler application while it was not under load. Afterward, I used the obtained values to generate new software. However, during testing on the motor pilot application, the motor does not start under load, regardless of...

TKara.2 by Associate III
  • 2667 Views
  • 6 replies
  • 0 kudos

Motor selection

Hello, I'm going to buy Nucleo-446RE and IHM08M1 board and do FOC position control.I'm going to analyze the code and practice using the ST Motor Control SDK.For questions, I would like to receive a recommendation for a motor that can be programmed wi...

SYJeong by Associate
  • 926 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.