STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

6 Step dead time problem

I can't see the dead time between the signals of the high and low MOSFETs of the same phase on the oscilloscope. The motor runs properly without load, but when a load is applied, the high and low MOSFETs of the same phase burn out. Photos and softwar...

TKara2_0-1740074458298.jpeg TKara2_1-1740074476284.jpeg TKara2_2-1740074500367.jpeg
TKara.2 by Associate III
  • 870 Views
  • 1 replies
  • 0 kudos

Motor Driver

I am using the EVLSPIN32G0A1 board to control a BLDC motor with the FOC / 6-step (trapezoidal) commutation algorithm with Hall sensor feedback. I have a few questions regarding its implementation and customization:1. Potentiometer Default Function: W...

KMaha.1 by Associate
  • 969 Views
  • 1 replies
  • 0 kudos

Resolved! Error at MCSDK workbench

Hello I had error during program generation at MC Workbench I attached the error log Please, let me know what is the problem kindly.Thanks SY 

SYJeong by Associate
  • 814 Views
  • 1 replies
  • 0 kudos

Incremental Encoder Alignment Problem

We are trying to control a 24V PMSM using ST Motor Control Workbench (MCW) version 6.3.1 with the FOC in order to control a sliding door. We are using “Position Control” as the control mode.We are using Nucleo-G474RE, STEVAL-IHM023V3 and X-Nucleo-IHM...

EDokm by Associate III
  • 1125 Views
  • 0 replies
  • 0 kudos

HSO firmware configuration

Hi, I have been working with the HSO motor control algorithm using Motor Workbench 6.2.0. I was able to successfully configure the firmware for a custom PCB, and it works correctly. The motor, which is a PMSM with 2 pole pairs, starts and runs withou...

RTirapegui_0-1729221267830.png RTirapegui_2-1729221502363.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.