STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Board Designer permitted crystal clock sources

Using Workbench 6.3.0.Creating an "inverter" board for a custom board which uses a 25MHz crystal. Only 8, 24, and 48 MHz crystals are offered in the dropdown. Can I edit JSON file to "clocksource": "25_crystal"? If not can I edit the CubeMx clock? Ca...

JoshS by Associate
  • 840 Views
  • 1 replies
  • 0 kudos

Resolved! EVSPIN32G4NH - opamp ADC setting

Dear community I would like to ask regarding ADC raw value for current sensing in STSPIN32G4. As we can see on below image the raw value of ADC1 CH3 and ADC2 CH12 is always in range of few hundreds. FYI, the motor is in rotating mode. We can see from...

image-20250212-085645.png image-20250212-090058.png Sheng123_0-1739353803676.png
Sheng123 by Associate II
  • 2165 Views
  • 1 replies
  • 0 kudos

MCSDK_v5.2.0 availability

Hello Everyone,We are working on a motor control, inverter drive strategy demonstrator unit using an STM32 MB1136 C-04 board.To start, we have a legacy example program for motor control, for which I could get the properly old CubeMX version, bit it a...

fszabi01 by Associate
  • 873 Views
  • 1 replies
  • 0 kudos

While Running Motor Starts Jerking.

Dear Experts,I need your help to figure out a problem in my MC configuration. I am using Nucleo-F401RE and a custom motor Driver board similar to STEVAL-IPM20B with 0.01R shunt resistor and opamp used it LM324. The current sense circuit in my custom ...

Screenshot from 2025-02-06 18-45-34.png Screenshot from 2025-02-06 18-45-42.png Screenshot from 2025-02-06 18-45-27.png Screenshot from 2025-02-06 18-45-49.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.